Dears,
Customers are looking for solutions based on the specifications below.
Could you check the solution?
Vin: 24VDC
Vout: 2output
a. 0~100Vdc
b. 0~ -100Vdc
Isolation : Need
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Hubert,
Please specify more in detail what exactly is meant with 0 to (-)100V. What is the regulation range that is needed for the positive and for the negative converter as well as the output current for the positive and negative output.
As long as the output power is not higher than roughly 100W, I recommend a flyback design, possibly with LM5155 or LM5156.