This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: Is its output current adjustable according to the external MOSFET?

Part Number: LM5176

Hi team,

Is its output current adjustable according to the external MOSFET?

customer input is 8-38V, output is 12V,

What can be achieved when the output current increases? Is it to replace an external MOSFET with higher current resistance?

  • Hello Amelie,

    Thanks for your question.

    Are you talking about the MOSFETs connected to the gate driver pins of the LM5176 (HDRV2, HDRV1, LDRV2 LDRV1)?

    Kind regards,

    Elisabetta

  • Hi Elisa,

    Yes.Does the load output current capacity of LM5176 depend on the MOSFET current  capacity?

  • Hello Amelie,

    The MOSFETs of the full bridge are usually chosen taking into account their RDSon and their gate charge in order to calculate the power losses that they might cause and they also need to have a VDS high enough wrt to the VIN. The MOSFET also need to be able to sustain the maximum peak current of the circuit and the maximum dissipated power not to get damaged. Usually all these info can be found in the datasheet of the MOSFETs.

    I would suggest to use the quick start tool to see if the chosen MOSFETs  are appropriate for your design  

     Kind regards,

    Elisabetta

  • Hello,

    I haven’t heard back from you, so I’m assuming you were able to resolve your issue. If not, just post a reply below (or create a new thread if the thread has been locked due to time-out).

    Thanks,

    Elisabetta