I applied a voltage to the ADC of UCD3138 in the range of 1.2V-1.5V.
The AD value showed a voltage about 20 mV lower(-1.5%) than the applied voltage.
I want to measure the AD value with high accuracy. Does an error of about 20 mV often occur?
I checked the data sheet'UCD3138 Highly Integrated Digital Controller for Isolated Power'.
Can the internal ADC reference voltage, ADC Zero Scale Error, and ADC Full Scale Error be the causes of the 20 mV error?
Is this error a variation or a normal deviation?
Is the error of the Internal ADC reference voltage included in the error of ADC Zero Scale Error and ADC Full Scale Error?