Other Parts Discussed in Thread: CSD18537NQ5A
Hi,
We use TPS2490 in a load switch configuration for switching a voltage of 40-50V with a drain current requirement is max 1A. The output load cap is 3000uF. The MOSFET used is CSD18537NQ5A.
We noticed that the device does not have a quick load discharge functionality. With 3000uF cap, its close to 0.15C charge at the output that needs to be dissipated in less than 2sec. Is their any other way we can achieve the same around this IC? We wish to avoid using a bleed resistor with a FET/BJT outside the IC.
Regards
Gaurav