Other Parts Discussed in Thread: BQ28Z610-R1, , TPS25750, TIDA-050047, BQ28Z610
Hello guys,
i want to create a USB C powered charger for bq28z610 and also bq28z610-R1 with different cell arrangement and charge parameters. My concern is, if I am using TPS25750 as USB Type-C handler and BQ25792 as charger (like TIDA-050047), the TPS25750 set the charging parameters for the charger, but how can the charger get the charging parameters from bq28z610 broadcast too? Can parameters set in TPS25750 be used as default, f.E. 4,2V 500mA, and the gauge delivers in addition 8,35V 1,5A while both I²C ports (from TPS25750 and bq28z610) are connected to the BQ25792 charge.
I guess this is quit too complicated without a microcontroller, so i will ask in an other way.
In a situation without the TPS25750 - Are bq28z610 and bq25792 compatible for an autonomous charge with the charge parameters in the bq28z610 registers? Under what conditions does the charger set the parameters (boot, periodically,..)?
Thanks in advice!