Hi team,
I'd like to know about the Ripple current.
My customer wants to use LM60440 for USB PD.
Since USBPD changes the output voltage, I am worried about the value of the output inductor.
Because Ripple current is less than 10% when input/output conditions are severe.
I think 10uH is good for my customer's condition.
However, the ripple current is severe under the following conditions.
Vin=20.4V
Vout=20V
Do I need to adhere to the minimum of 10% stated in the datasheet?
What happens if you don't follow it?
Sincerely.
Kengo.