I am designing in WEBENCH using the LM61440-Q1. WEBENCH is indicating PFM operation anytime the Ipp percentage goes over 50%. It seems to me that it should not go into PFM mode until Ipp percentage is greater than 200% (i.e. Ipp is more than twice Iavg). Is this a bug in WEBENCH? Is there any way to estimate the efficiency at low load while still operating in CCM mode?