This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LV2862: with PoE issue

Part Number: LV2862
Other Parts Discussed in Thread: LMR36506

Hi sir,

I use the LV2862 application on the PoE step-down circuit.

Vin = 57V / 0.028A Vout = 3.3V / 0.4A

I use TI Webench to simulate circuit parameters, but the Ethernet does not work properly.

So I changed the capacitance of Cin / Cout, when Cin = 10uF/100V Cout = 22uF*4, the network can operate normally.

I have the following questions to ask,

1. Is this solution possible? Will there be other risks?

2.Why refer to the Webench value, which will cause the network to not operate normally. LV2862.pdf

Cin L1 Cout Vout network
10uF 27uH 22uF 3.3V No connection
20uF 27uH 22uF 3.3V No connection
30uf 27uH 22uF 3.3V No connection
10uF 47uH 22uF 3.3V Internet intermittent
20uF 47uH 22uF 3.3V Internet intermittent
30uf 47uH 22uF 3.3V Internet intermittent
10uF 47uH 22uF*4 3.3V Network OK