This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM53604: Application of negative output

Part Number: TPSM53604


Hi,

I will plan to use TPSM53604 for negative output. Refer to the document as below. I am no idea about the value of Cbulk. Would you help to suggest the better value of Cbulk?

www.ti.com/.../snva897

Thanks,

CC

  • Hi Chen,

    You can use a 100uF bulk cap with high ESR (10-30mOhm). This will help dampen input voltage ripple and any noise that is a result of having long input leads. 

    Here's an example of a 100uF bulk cap ().

    Regards,

    Jimmy