Hello team,
TPS7B4254-Q1 has thermal information as below.
RθJA Junction-to-ambient thermal resistance 45.4 °C/W RθJC(top) Junction-to-case (top) thermal resistance 51.1 °C/W RθJB Junction-to-board thermal resistance 27 °C/W ψJT Junction-to-top characterization parameter 8.2 °C/W ψJB Junction-to-board characterization parameter 26.9 °C/W RθJC(bot) Junction-to-case (bottom) thermal resistance 6.4 °C/W
Can I get maximum(worst case) value for this?
I haven't seen any datasheet in TI which includes min, typ, max for thermal resistance. The thermal data on datasheet guarantee worst case?
Thanks.
Regards,
Oliver Kim