Hello,
I have a question about the datasheet [7.8 Logic interface Characteristics].
The output low level test condition is Ipullup = 3mA.
Do I need to flow Ipullup=3mA as well?
In LP 5569 EVM schematic, VIN = 3.3 V Rpullup = 6.04 k,
so Ipullup = 0.55 mA.
Ipullup=3mA might not be necessary?
If there is a recommended current value, please let me know.
Best regards,
Hyodo