This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Stuck in Status 0x05

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQSTUDIO, GPCCHEM, BQ34Z100

Hi again,

after changing parameters, trying to get Status 0x05, reprogramming the device so I can change the values in data memory againg because i was stuck in Status 0x04 i finnaly made Status 0x05 last Friday.

But now I am charging, relaxing, discharging, relaxing the 3rd time and I can't get status 0x06. These points I think are a bit wired:

  • I see the Grid Number is going up while discharging, but I can't remember that I have ever seen a higher number than 10
  • In the relax after discharge phase the Volt is going down, down, down until it has really no power more. Then The BQStudio can't connect to the BQ34Z100G1 anymore. The Battery is still connected to the EVM but no Charge or discharge-resistor are connected on the 3. Pin.
  • The "True RC" and "True FCC" doesn't shows the correct value always but after the (I think) discharge phase it shows the real mAh for my battery Pack. But the "Remaining Capacity" and "Full Charge Capacity" only shows a 1/4 of the real Capacity.

But nevertheless with my "I think" and "remember", I have attaced the log and the "SREC" File for you to see whats my problem.

Scenario: I've got 8 Panasonc "Eneloops" BK-4MCCF in series. ChemID: 0644. All other Data Memory configuration should be availabe in the ZIP File.

I really hope you guys can help me.

Benjamin5265.OutputFiles.zip