This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2705: The limit for the LM2705 FB pin upper resistance

Part Number: LM2705
Other Parts Discussed in Thread: TLV61048, LM27313

Hi 

Is there has a limit for the LM2705 FB pin upper resistance?

For TLV61048 as an example, the upper limit of voltage divider R2 must not exceed 150K ohm.
Because this parameter will affect the power consumption.

Besides, can you help confirm whether the power chock can use 4.7uH, and the overall power consumption is about 5mA? Did LM2705 has the calculation file? I can't found this part in the WEBENCH, thanks.