hi,
We are currently using bq25606 power management IC In our design which has a load requirement >2A.
for battery monitoring we are using max17260. We are facing few issues with the system and have below queries to be cleared.
Observation:battery charging takes time when system is ON(load of 2A connected to vsys)
1.Is management IC capable of performing charging functionality parallel with load connected?
2. should we keep the system off(load disconnected) during battery charging?