I was troubleshooting a design that uses the TPS56C20, and had ringing in some conditions (5-10kHz ringing on output - obvious as audible inductor whine). It seemed to be related to my test setup & large inductance leads. But I then noticed a ringing around the same frequency on turn-on (much shorter - but still present) after changing around the load setup.
I'm seeing ringing on the device during power-on. It's more noticeable at certain loads (often ~3-6A), but seems to always be present. Using the dev board "fresh from the box" I discovered it also happens there too (my next step in troubleshooting was getting a "known good" example) - see these photos:
On my own board - if I slow down the turn-on time by changing the SS capacitor, you still get it even with an insanely slow turn-on time Yes that's 200ms/div):
Going back to the dev board, here is my setup:
I get this ringing regardless of input voltage and for many current settings. The load is a DL3021. Is the test setup wrong somehow or is this an issue with the part?
One caveat is I *need* to use the programmable VCC-INT feature so don't want to use just an external feedback network. But I was seeing this problem with both the default internal & external feedback options. I didn't seem to find a lot of details in the datasheet on actual stability information besides the recommended values.
Appreciate any thoughts - whether official TI or anyone else who has seen something similar. I assumed it was just my quick prototype design issues until I recreated on the dev board!
Thanks,
-Colin