Hi,
A customer wants to make a portable electronic product. I am looking for a Boost converter with the spec below, but there are conditions.
There are situations where the current needs up to 12A, but is there a boost converter that can be set to output 9A as a continuous current?
Vin : 3.7V
Vout : 5~6V
Iout : 9A
In the above conditions, 12A is required, but because 9A is output, the protection for the current limit should not work.
If there is a suitable product, please recommend it.
Thanks.
Regards,
MJ