I plan to design the circuit using BQ25616 and typ-C connector.
I want to support typ-C Current without implementing PD support.
Can the following design be used?
・ VBUS, D +, D- are connected to BQ25616
・ CC1 and CC2 are pulled down with 5.1kΩ
・ GND is connected to GND on the board
・ Other terminals are open