This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3707: About generation of heat

Part Number: UC3707


Hello

In UC3707, VIN = Vc = 40V.
When the input signal is 3.3V / 40KHz / Square wave, the device heats up considerably. It seems to be about 50-60 ° C.
Is this normal?
Do you have data on thermal characteristics?

  • Nakasone -san,

    Thank you for reaching out!

    This may have something to do with what you are driving.

    1)  What are you driving?  If they are FETs, what is the gate charge (Qg)?

    For each channel, the gate drive power can be calculated by:  P_Drive = Qg x Vc x Fsw        (Multiply by 2 for total power)

    If the power dissipated is high and you are using no gate resistors; consider using low value resistors (~ 1 Ohm to ~ 5 Ohm) to help dissipate some of the power.  This will increase turn-on and turn-off times slightly as a consequence.

    Regarding thermal characteristics; I do not believe they are available.

    I look forward to hearing back.

    Thanks,

    Aaron Grgurich

  • Hello Grgurich-san

    I have now created an evaluation board and it is working with the UC3707.
    The application is thinking of driving an ultrasonic sensor.
    It is not a FET.
    The output is unconnected (oscilloscope only) or an ultrasonic sensor is connected.
    This is an excerpt from a magazine, but the image is as follows.(+12V →6~40V)
    Please let me know if you have any notes
  • Nakasone -san,

    Understood.  Looking at the schematic, the AC coupling capacitor (0.1uF) is a large load.  This is very likely why your part is getting hot...

    The AC coupling capacitor probably will not be seen completely as a load, so for a rough calculation you can reduce / calculate this number more accurately by knowing how the load affects it (you will need to know the capacitance of the load too).

    Using the Gate Power Equation below, we can see why the gate driver is getting so hot.

    P_g = (0.1 uF)*((40 V)^2)*(40 kHz)  = 6.4 W

    Even if we half the capacitance, we can see that the driver must dissipate 3.2 W.

    I hope this makes sense as to why the gate driver is getting so hot.  If this answered your question, please click the green button, otherwise feel free to follow up!

    Thanks,

    Aaron Grgurich