Hello guys,
One of my customers is considering using TPS25221 for their next products.
They have the following question about RILIM. Could you please give me your reply?
Q. We'd like to set 1.0A as ILIM. According to Figure 24, Current-Limit Threshold vs Current-Limit Resistor (RILIM) on page 14 of the device datasheet(SLVSDT3D),
RILIM(typ) is about 55kohm for 1A. Also the ILIM variation range is about 900mA~1100mA.
While RILIM(typ) is about 974mA for 1A acoording to equation (1) on page 14. Also the ILIM variation is 721mA~1328mA.
My question is the below.
Which is closer to the actual current? the graph or the equation?
?
Your reply would be much appreciated.
Best regards,
 Kazuya.