HI,
Is there a problem in using the TPS3808G25 if VDD is 3.3 V. The table in chapter 5 in the data sheet, indicates that one should use TPS3808G33. The note under the same table says "Custom threshold voltages from 0.82 V to 3.3 V, 4.4 V to 5 V are available through the use of factory EEPROM programming" and the recommended operating conditions says VDD up to 6.5 V, not refering to the table in chapter 5.
Can it cause any problems using TPS3808G25 on VDD=3.3 V except that the threshold voltage will be lower than in the 3.3V version??
Thanks in advance!