Hi,
The datasheet of the TPS22810 does not explicitly mention that the thermal pad of the WSON package can be shorted to the circuit ground (e.g. shorted to pin 4). In the schematic of the TPS22810EVM module I see that this is done, but I want to be 100% sure. Can you confirm that the thermal pad can be connected to circuit ground?
Thank you