Other Parts Discussed in Thread: BQ25883, BQ40Z60, , BQ34Z100-G1
Hello,
This is my 1st time designing a circuit that incorporates a Li-Ion battery, and I need some help.
The circuit I'm designing needs only 3.3V. And so, I thought of 2s 18650 Li-Ion batteries feeding a switching regulator. The circuit has an LCD display, and it should show the battery charge percentage (State of Charge / fuel gauge) on its top-right corner. And the circuit will have a 5V power input connector, from where it will get power to run if connected and also from where it'll get power to charge the battery. If there's no 5V on the power input connector, the circuit should then get its power from the battery.
So, after studying TI solutions, I thought of using the BQ28Z610 (Battery fuel gauge with integrated protector for 1-2 series packs) to get State of Charge of the battery, and the BQ25883 (2-Cell, 2-A Boost-Mode Battery Charger With Power Path, USB On-The-Go Boost (OTG) For USB Input) for charging the battery.
1st question: Are those good choices for my needs?
I tried to find a 1-chip solution, and found the BQ40Z60 (Programmable Battery Management Unit), but it costs $15 USD on Digikey, and require a large amount of external components.