This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61391: IBIAS min/typ/max depending only temperature variation

Part Number: TPS61391

Hello,

 

My customer would like to know IBIAS min/typ/max variation over temperature to confirm they have to calibrate it depending on temperature. Though datasheet specifies IBIAS min/typ/max variation all over PVT is 15/20/25uA, Considering only temperature variation, how much they would be respectively?

(For variation depending on power supply voltage and device variations, they can calibrate them at power up, but for temperature variation, they may need to calibrate it during operation on the fly. To judge if they have to do that or not, they are asking this question.)

 

Best regards,

 

K.Hirano