Hi,
I'm finding a reset IC.
VDD : 4V
reset time : 10s
I saw the TPS3808 but it doesn't support 4V supply voltage.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello SY,
When using TPS3808G01, you need to use an external divider to monitor the voltage as shown below.
Doe TPS3808G01, the SENSE pin comparator voltage threshold is 0.405V. You can design R1 & R2 such that for Vin > 4V, the RESETz is not asserted. When Vin goes below 4V, the SENSE pin voltage goes below 0.405V and then the RESETz is asserted.
The RESET delay can be programmed by connecting a suitable capacitor on CT pin. Refer section 8.3.2 of datasheet for capacitor selection.
Apart from TPS3808, following other options may be useful to you.
1. TPS3899DL01DSER - This device also needs external resistance divider similar to TPS3808G01. It's internal threshold for SENSE pin is 0.505V. Additional benefit with TPS3899 device is, it allows programmability for SENSE delay as well as RESET delay using capacitance.
2. TPS3840DL40DBVR - This device will monitor the VDD voltage. It does not need resistance divider. When VDD goes below 4V, the RESETz will be asserted. The RESET delay can be programmed by external capacitor on CT pin.
Thanks & Regards,
Shridhar.
Hello SY,
Somehow the external resistance divider image does not show up in my previous reply.
Please refer Figure 8-1 in TPS3808 datasheet for the image.
Thanks & Regards,
Shridhar