This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610-R1: SOC is 97~98% after charging complete

Part Number: BQ28Z610-R1

Dear Sir,

SOC is displayed 97~98% after Charging complete. not reach 100%.

Could you please let me know check point.

please refer GG file.

Setting value

Charger IC

  • Charging Voltage : 4.162V
  • Charging Current : 2A
  • Termination Current : 100mA

BQ28Z610-R1

  • Charging Voltage : 4.16V
  • Termination Current : 100mA

EK430_Golden Image_20210129.gg.csv