Hi,
I have several queries with regards to LP8725. It is as follows:
1) The DVS voltage on the BUCK1, can it be set to any desired voltage that is set into the register REG 0x08[4.0] and REG 0x09[4:0]?
Eg:
REG 0x08 programmed to 1.2V, REG 0x09 programmed to 1.1V
Toggling the DVS pin will make the BUCK1 output to have 1.2V or 1.1V according to the high and low state
.
REG 0x08 programmed to 1.1V, REG 0x09 programmed to 1.0V
Toggling the DVS pin will make the BUCK1 output to have 1.1V and 1.0V according to the high and low state
If my processor DVS needs 3 voltages 1.2V, 1.1V and 1.0V, are we able to load the desired voltage settings into the REG 0x08 or REG 0x09 and toggle the DVS pin to get the desired output voltage?
2) What is the time it takes to switch from one voltage to another voltage (Settling time)?