Other Parts Discussed in Thread: ATL431
Hi team,
Could you tell me the meaning of continuing the absolute maximum rating?
Does a very short pulse increase the acceptable range?
If you have any conditions, please let me know.
Sincerely,
Kengo.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Marcoo,
Thank you for your reply.
I'm sorry if I may have been unclear.
I'd like to know about the meaning of the continuous cathode current range for IKA.
My customer the peak current exceeds the absolute maximum rating for a moment.
Is there a regulation for the maximum value of peak current?
Sincerely.
Kengo.
Hi Kengo,
What type of application is this ATL431LI used for?
What is the function in that application?
We offer the ATL431 that has 100mA IKA maximum if you have issues with the ATL431LI 15mA.
I cannot recommend any current value above ABS MAX even if it is a pulse. If the pulse is short, can you add capacitors to kill the pulse transient to make it lower than abs max?