Im going to desing synchronous buck converter using TL494 with input voltage is 20V, output voltage is 5V and output current is 2amp. I wil use one two input mosfet driver(high side and low side mosfet driver) to controll the two mosfet in main buck converter circuit. Now can i take connection one from collector(pin8) and one from emiter(pin10). For tight the output i want to connect pin 11 with pin 8 and pin 9 with pin 10. will it work? Thank u