This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: During short circuit condition

Part Number: LM5069

Hi,

What limits the output voltage during the the short circuit condition.

Its goes into a restart mode if the short circuit is permanent, what determines when to turn off after every restart.

The current limit was set to 18A, the voltage rail is 50V, the short circuit was simulated using 2R2 power resistor.

The output voltage reaches to ~4V before the Hot swap disabled it. the current through the resistor is around ~ 2A during every restart.

Thanks

Siva