Other Parts Discussed in Thread: TPS7A84A
Hello experts,
My customer plan to use TPS7A8300 to provide current for two loads.
One load's average current consumption value is about 700mA but peak current value is about 1.4A. The other load is same one.
So, average current consumption should be 1.4A and peak current value might be 2.8A in worst case.
Can TPS7A8300 support this condition?
From datasheet, output current limit is 3.4A(typ), so I thought TPS7A8300 can endure for peak current 2.8A
I would appreciate if you would give me comment.
Thanks and best regards,
Ryo Akashi