Other Parts Discussed in Thread: BQ25600,
Dear All
We have one question for can't charge done issue of BA25601.The pin9 STAT voltage always low even the charging with low time.
I have testing charge with four devices at room temperature.
2pcs devices are okay,battery voltage =4.052V and STAT change to high
2pcs device are fail, battery voltage = 4.041V & 4.042V and STAT always low even charging time over all night.
Could you help to check SW swtting and HW design?
--------------------------------------------------------------------------------------------------------------
software register as below:
I2C_ByteWrite(BQ25601_ADDRESS, BQ25600_REG00,0x1F);//Input Curent Limit 3.2A
I2C_ByteWrite(BQ25601_ADDRESS, BQ25600_REG02,0x82);//0.12A Charge
I2C_ByteWrite(BQ25601_ADDRESS, BQ25600_REG03,0x00);// Termination Current Limit:0.06A, Pre-charge Current Limit:0.06A
I2C_ByteWrite(BQ25601_ADDRESS, BQ25600_REG04,0x30);
I2C_ByteWrite(BQ25601_ADDRESS, BQ25600_REG05,0x8F);
-----------------------------------------------------------------------------------------------------------------