This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5155: LM5155 boost

Part Number: LM5155

dear

      The design requires 10V low voltage protection, other voltage power requirements normal.After using the UVLO function, the output voltage of 10-12V will decrease linearly, and the efficiency is only 50% when it reaches about 11V, which is lost in the MOS tube.Is this state normal?

    any advance?thanks in advance~