Hi Team:
There is laptop application question when used with a bad battery as for BQ25710, could you help to give your comments, thanks!
> The battery is a bad one(output voltage is 0V), so the function of charging and discharging function are disabled, but I2C communication is ok.
The CELL BATPRESZ is 4.5V, 4cells , then EC can not detect the battery voltage, so EC write Regs of Charger Regs 14h/15h/3Eh as 0A/8.8V/5.9V, but when measure the VSYS and BFET at this stage, just find VSYS is 5.9V, BFET is off.
Question 1 is :Why this stage VSYS is 5.9V instead of 8.8V?
Question 1 is :Does VSYS drop to 0V because of VSYS voltage 5.9V (2cell value) not matching CELL_BATPRESZ(4cell config)?