Hi. there.
I'm DH.Kim
I'm reviewing the totem pole PFC using TIDA-00961.
and attached file is the circuit of TIDA-00961.
please see the attached file and page 2(two) with UCC27712DR(U102)
there are L1 and H1 in I.C
The input PWM from DSP is that LI is from Si_Gate_H and HI is from Si_Gate_L.
But, I think, LI is from Si_Gate_L, HI is from Si_Gate_H.
I'm a little bit confused. Please let me know which one is correct.