This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100EVM: After Programming wrong detachted Device?

Part Number: BQ34Z100EVM
Other Parts Discussed in Thread: BQ34Z100, EV2400, BQSTUDIO,

Hi,

I was trying to do a correct learning curve. And after I found out I had set a wrong parameter (which can't be set after in IT_Gauge Mode) I decided to start from the beginning. So I ReProgrammed the BQ34Z100 over the EV2400 (newest version) with the bq34z100_G1_v0_16_build_17.srec which I have downloaded here at TI (I've done this a few times without any issues). But now I can't get anything working again.

Restarting BQStudio the device couldn't be found correctly (which it did until now). It also states it has Auto Detected Device : 0001_0_02 @ 0x16 (Normally it's 0100_0_16 on Addr: 0xAA).

It looks like the programming has crashed the BQ34Z100. I am still able to reprogramm with the above image file but it is still now working.

Is there any way to completly reset the BQ34Z100EVM? Or maybe it's the EV2400 which doesn't work correctly?

Thanks for your help