Part Number: BQ78350
Other Parts Discussed in Thread: BQSTUDIO, ,
Hi,
We want to program and calibrate the bq78350 with our own SW Tool because using Battery Management Studio is extremely manual, and is not suitable for mass production.
I did not find a clear documentation to transfer a golden image (srec file) to the bq with own software tools. So I have the following questions / problems:
Question 1: Is there any recommendation on how to program the bq78350 from the .srec file, in a way that can be automated?
Question 2: Is there any recommendation on how the bq78350 can be calibrated without using bqstudio?
Question 3: Do you have any suggestions for interfaces / tools / libraries that can be used with Python, with the bq78350?
Thanks, Tom
I have seen other similar questions on the forum (link), and see that some information was sent in a private message... Would it be possible to get this information? I have already read the other documentation etc. linked in this post.