Other Parts Discussed in Thread: LM5146, LM5117-Q1
Hi,
Please see attached preliminary PDF schematic which shows one of two Buck Converters.
I am trying to use two LM5146 as variable current sources using local output shunts to create the voltage feedback. The shunt output is fed back to an error amp with a variable reference to provide a variable setpoint.
The question is can the LM5146 "comp" pin be driven directly to produce the signal to the PWM generator and bypass the internal error amp? If not, is there a more suitable chip? I was considering using another amplifier to provide offset and gain to drive the internal amplifier, but would rather not.
Thanks for the help.
Don