This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5569: current consumption

Part Number: LP5569


Hello,

Please let me know if the current consumption of LP5569 is the same or not.
Current consumption when LEDx is OFF,


ex.LED1 OFF
a, 17h LED1 _ PWM  FFh  and  23h LED1_CURRENT 00h
b, 17h LED1 _ PWM  00h  and  23h LED1_CURRENT AFh
Is there a difference in the current consumption of LP 5569 in a and b states?

Best Regards,

Hyodo

  • Hi Hyodo,

    Operating in the same current status, analog dimming will cost more consumption than PWM dimming.

    So the consumption between the two status are different and status b will cost more(When the LEDx is in the OFF status, the difference of consumption is smaller than in the ON status).

    Best Regard 

    Monet Xu