Part Number: TPS63806
Other Parts Discussed in Thread: SN74CB3T3245, TPS63811, TPS63810, TPS63805
Hello,
Based on the WEBENCH it is possible to use the TPS63806 to stabilize the FPGA VCCIO 3.3V from 3.0V to 3.6V input voltage, but since no simulation can be done using WEBENCH for this device, I want to verify that the TPS63806 can be used for that purpose.
Can I use the TFM201610ALC-R47MTAA Inductor from TDK with TPS63806 ?
Thanks!
Yossy Goldenberg