We want to design a charging base to charge two game handles at the same time
The specific requirements are as follows:
1. Input voltage: it can be VBUS or AC adapter
2. The output interface is type-c
3. The maximum charging current of each handle is 1.4A
4. Charging status indication (charging, charging completed, charging fault)
5. The charging current can be regulated independently as far as possible (trickle charging / pre charging / constant current charging / constant voltage charging, and the voltage and current limits can be set independently)
5. Charging protection function (overcharge / overtemperature / OCP, etc.)
Is there a suitable IC to recommend? Is there a reference line to provide? Thank you