Other Parts Discussed in Thread: BQ34Z100, , BQSTUDIO
Hi,
We are using BQ34Z100 as a gauge-meter along with BQ25713 as part of main charge control IC in our battery back up based design.
Battery used is 2-terminal 3SP1 with 10.7V as max voltage.
Currently we are performing learning cycle and to capture the log information we are using BQStudio.
We captured the log while battery is charging, initially charging current was 370mA and as state of charge increased,0434.battery_charge_log.csv charge current got decreased (below 50mA), because of that it was taking more time to charge the battery.
Please find the attached .csv file for the same.
We are using following register setting
ChargeCurrent() [Reg 0x03/02] - 1A
ChargeVoltage() [Reg 0x04/05] - 10.7V
InputVoltage() [Reg 0X0B/0A] - 2V
IIN_HOST() [Reg 0x0F/0E] - 3.3A
MinSystemVoltage() [Reg0x0D/0C] - 10.7V
Could you please give any solution on how to increase charging current ?
Thanks and Regards,
Sudha Nayak