This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27742-G1: Remaining uncompensated battery capacity and SoC decreases rapidly after a few cycles

Part Number: BQ27742-G1
Other Parts Discussed in Thread: BQSTUDIO

Hi,

Our product uses a rechargeable Orbtronic 3400 mAh battery:
https://www.orbtronic.com/protected-3400mah-18650-li-ion-battery-panasonic-ncr18650B-orbtronic

We are noticing that, in about 10% of our production devices, the uncompensated battery capacity decreases rapidly after about a dozen cycles. The capacity starts 3200-3400 mAh and then it becomes 1500-2000 mAh at which point the charger indicates that the battery is fully charged. The state of charge (SOC) is also reported around 40-50% when the battery is fully charged.

Please note that the indication of the battery being fully charged is done by part number BQ25898YFFR.

We can mitigate this issue by either sending Control() [RESET] subcommand or reprogramming the golden image (with the same image as before). This seems to default the capacity and SOC values.

Is this behavior by design or could this be an existing issue? Could this also be a matter of misconfiguration?

Please let me know if I can provide more information.

Thank you.