Part Number: UCC28C44
Other Parts Discussed in Thread: UCC24612
Hi,
I´m using the UCC28C44 for my Flyback application. The switching frequency is 1MHz and the Output 5V / 2A.
With the webench power-designer the efficiency is 78%.
Is there a possibility to use a synchronous rectifier controller with the UCC28C44 to increase the efficiency?
Best regards
Emanuel Lemnitz