Part Number: BQ34Z100EVM
Other Parts Discussed in Thread: BQSTUDIO, EV2400
I've been using BQ Studio to change a parameter on the Gas Gauge but get the message " A read of data written failed comparison". In my application the capacity of the battery isn't being updated which I believe is because the Cell Terminate Voltage is set to low.
If I try to change it from anything other than the currently set value I get the error message as per the attached screen shot. The Eval kit is connected to Windows 7 Laptop with the EV2300 programmer over I2C, I can see the device and the status, it also reads the data memory fine. I don't think the device is sealed, I have pressed the unsealed button to be sure but this didn't seem to make any difference.