Other Parts Discussed in Thread: LM3409
Hello, we have a question to ask, here is, we are doing design high current LED drive PCB, customer assigned to use LM3409HV, the VIN = 48v , one LED only with PWM dimming control, VF LED = 3.5v , ILED=3A , for efficiency consideration, do we need to use a buck PWM controller to switch 48v VIN to 6v to provide to LM3409HV (LM3409HV Vin min. = 6v) or we could input 48v to LM3409HV directly (due to 48v to drop to VF LED 3.5v, ILED 3.5A, is there efficiency and power dissipation issue of LM3409HV) ?
Best regards,
Ekozy Sam