Other Parts Discussed in Thread: LM74800-Q1, INA302, LM74610-Q1
Hello everyone,
I want to build a test circuit based-on Design TIDU415: 24-V DC,10-A eFuse, and Protection Circuit for programmable Logic Controllers (PLC). The core components are the LM5069 and LM5050. However, I need that all the components are automotive-grade I didn't find in the catalog the matching part with that spec. Is there similar part numbers I could use?
Moreover, for my scenario the max-load could be up-to 24V@40A.
Do you guys have any suggestion?
Thanks!