Other Parts Discussed in Thread: TPS2830, LM5104,
Hello,
Following on from my previous post:
Upon extensive further testing, we found that at higher operating frequencies (<100kHz), the pulling down of the bridge via a resistor was not suitable and we ended up with the same issue as originally described (low side MOSFET not switching on due to bridge voltage not going low enough).
An additional solution that we have thought about is controlling the DT pin based on a delayed signal going to the input pin. In the schematics below I show how we propose that this would be done (JP6 would be not fitted), the DT pin is receiving the same signal is a IN pin with a 100ns delay.
Are there any issues with running the IC in the proposed configuration? anything else that we would need to consider?
Are there any other MOSFET drivers based on technology as the TPS2830 or TPS2834? our operation criteria leads us to stay away from CMOS technology whenever possible hence why other MOSFET drivers such as the LM5104 cannot be used.
Thank you in advance for your response.