Hello team,
I have questions about input and output capacitor selection written in LMZM33604 datasheet p.17.
- Input capacitor selection
Datasheet states minimum 20uF is required.
- Is the value of 20uF effective capacitance value after taking DC bias into account?
- or Does this mean that it requires at least two 10uF(50V) cap such as C3225X5R1H106K recommended in table2 regardless of input voltage?
- Output capacitor selection
table3 shows minimum required Cout.
- Is the capacitance value in the table effective capacitance value after taking DC bias into account?
- or is it fine without considering DC bias derating if capacitor's voltage rating is equal or higher than the listed value?
Best regards,