This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65192: TPS65912: SPI Protocol

Part Number: TPS65192
Other Parts Discussed in Thread: TPS65912

From datasheet, it stated that TPS65912 supports both SPI and I2C interface.

When configured to use SPI interface, can SPI access all the TPS65912 register ? 

Section 7.18 stated that the host to access interrupt status register via I2C ? 

  • Hello May,

    Let me assign this to correct product line that supports TPS65912 device and someone will respond to you soon.

    Kind Regards,

    Liaqat

  • Hello May,

      Yes, the SPI can access all the TPS65912 registers. Please see section 7.22 below: 

    7.22 Interfaces

    There are three interfaces in the TPS65912x device. A high-speed I2C interface that has access to all register, a SPI interface that can optionally be used to access all registers and a high-speed power I2C interface that can be used to dynamically change the output voltage of the DC-DC converters. The power
    I2C interface only has access to the voltage scaling registers of the DC-DC converters.