This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542-G1: 0degC or 5degC low temp charge, charge current is 0.2C,SOC 0% will be held long time for about 3~5h

Part Number: BQ27542-G1
Other Parts Discussed in Thread: BQ28Z610-R1

Dear Teams,

We need your helps,the question we have not solve it for a long time.

We find when battery charge at 0degC or 5degC low temperature, SOC 0%  will be held long time for about 3~5h。

We have tested 3 project,capacity are 5000mAh,5800mAh and 15000mAh,charge curreng is 0.2C(1000mA,1160mA,3000mA),SOC 0% hold 3h and 5h

But we test another project with bq28z610-r1 gauge IC,capacity is 3850mAh,charge current is 770mA,SOC 0% hold time is less than 1h.

We find it is not chem ID issue,maybe is the gauge IC itself issue.

Atached file are the 3 project test log data,please check.

Thank you.15000mAh system battery 5degC 0.2C charge.log15000mAh system battery 0degC 0.2C charge -1.log256009-B 5degC 0.2C charge.log256010 0degC charge-4.3V -1.log